Statusword
|
15 |
14 |
13 |
12 |
11 |
10 |
9 |
8 |
7 |
6 |
5 |
4 |
3 |
2 |
1 |
0 |
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
|
Manuf. specific |
Op. mode specific |
Int. limit active |
Target reached |
Remote |
Manuf. specific |
Warning |
Switch on disabled |
Quick stop |
Voltage enabled |
Fault |
Operation enabled |
Switched on |
Ready to switch on |
||
|
O |
O |
M |
M |
M |
O |
O |
M |
M |
M |
M |
M |
M |
M |
||
| Bits | Definition | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
| Bits 0,1,2,3,5,6 | Device state (see table 1) | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Bit4 | High voltage is applied to the drive (if bit is set to 1) | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Bit5 | If this bit is equal to 0, the drive is reacting on a quick stop request. | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Bit7 | If this bit is set to 1, a drive warning is present. The cause means no error but a state that has to be mentioned. The status of the drive does not change. The cause of the warning may be found by reading the Warning_Inserted (59A2.0H) object. This bit is set and reset by the device. | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Bit8 |
This bit may be used by a drive manufacturer to implement any manufacturer specific functionality. |
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Bit9 | If this bit is set to 1, then parameters may be modified via CAN-network and the drive executes the content of a command message. If this bit is equal to 0, then the drive is in local mode and will not execute the command message. In local mode the drive will accept accesses via SDO. | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Bit10 | If this bit is set to 1 then a set-point has been reached. The set-point is dependent on the operating mode. The description is in the chapter of the specific Operation mode. | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Bit11 | This bit indicates that an internal limitation is active. | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Bits 12,13 | These bits are operation mode specific. The description is in the chapter of the special mode. | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Bits 14,15 | These bits may be used by a drive manufacturer to implement any manufacturer specific functionality. | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Bit6, Bit5, Bit3, Bit2, Bit1, Bit0 |
These bits indicate the status of the device:
|
Statusword for commands:
Statusword for Interpolated Position Mode (ip)
Statusword for Profile Position Mode (pp)
Statusword for Homing Mode (hm)
Statusword for Profile Velocity Mode (pv)
Statusword for Cyclic Synchronous Position Mode (csp)
Statusword for Cyclic Synchronous Velocity Mode (csv)
Statusword for Velocity Mode (vl)
Statusword for Profile Torque Mode (tq)
Statusword for Cyclic Synchronous Torque Mode (cst)
Statusword for Feedback Sensor Calibration Mode (fsc)
Statusword for Interpolated Position Mode (ip)
|
15 |
14 |
13 |
12 |
11 |
10 |
9 |
8 |
7 |
6 |
5 |
4 |
3 |
2 |
1 |
0 |
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
|
Manuf. specific |
Operation mode specific |
Internal limit active |
Target reached |
Remote |
Manuf. specific |
Warning |
Switch on disabled |
Quick stop |
Voltage enabled |
Fault |
Operation enabled |
Switchedon |
Ready to switch on |
||
|
O |
O |
M |
M |
M |
O |
O |
M |
M |
M |
M |
M |
M |
M |
||
|
X |
X |
reserved |
Ip mode active |
X |
Target reached |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
|
Bit |
Name |
Description |
|
|---|---|---|---|
|
10 |
Target reached |
0 |
Halt = 0 : Position not (yet) reached Halt = 1 : Motor in deceleration |
|
1 |
Halt = 0 : Position reached Halt = 1 : Motor speed zero |
||
|
12 |
Ip mode active |
0 |
Interpolated position mode inactive |
|
1 |
Interpolated position mode active |
Statusword for Profile Position Mode (pp)
|
15 |
14 |
13 |
12 |
11 |
10 |
9 |
8 |
7 |
6 |
5 |
4 |
3 |
2 |
1 |
0 |
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
|
Manuf. specific |
Operation mode specific |
Internal limit active |
Target reached |
Remote |
Manuf. specific |
Warning |
Switch on disabled |
Quick stop |
Voltage enabled |
Fault |
Operation enabled |
Switched on |
Ready to switch on |
||
|
O |
O |
M |
M |
M |
O |
O |
M |
M |
M |
M |
M |
M |
M |
||
|
X |
X |
Following error |
Set-point acknowledge |
X |
Target reached |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
|
Bit |
Name |
Value |
Description |
|---|---|---|---|
|
10 |
Target reached |
0 |
Halt = 0 : Target Position not reached Halt = 1 : Axle decelerates |
|
1 |
Halt = 0 : Target Position reached Halt = 1 : Velocity of axle is 0 |
||
|
12 |
Set-point acknowledge |
0 |
Trajectory generator has not assumed the positioning values (yet) |
|
1 |
Trajectory generator has assumed the positioning values |
||
|
13 |
Following error |
0 |
No following error |
|
1 |
Following error |
Statusword for Homing Mode (hm)
|
15 |
14 |
13 |
12 |
11 |
10 |
9 |
8 |
7 |
6 |
5 |
4 |
3 |
2 |
1 |
0 |
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
|
Manuf. specific |
Operation mode specific |
Internal limit active |
Target reached |
Remote |
Manuf. specific |
Warning |
Switch on disabled |
Quick stop |
Voltageenabled |
Fault |
Operation enabled |
Switched on |
Ready to switch on |
||
|
O |
O |
M |
M |
M |
O |
O |
M |
M |
M |
M |
M |
M |
M |
||
|
X |
X |
Homing error |
Homing attained |
X |
Target reached |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
|
Bit |
Name |
Value |
Description |
|---|---|---|---|
|
10 |
Target reached |
0 |
Halt = 0 : Homing position not reached Halt = 1 : Axle decelerates |
|
1 |
Halt = 0 : Homing position reached Halt = 1 : Velocity of axle is 0 |
||
|
12 |
Homing attained |
0 |
Homing mode not yet completed |
|
1 |
Homing mode carried out successfully |
||
|
13 |
Homing error |
0 |
No Homing error |
|
1 |
Homing error occurred. Homing mode carried out not successfully. The error cause is found by reading the error code. |
Statusword for Profile Velocity Mode (pv)
|
15 |
14 |
13 |
12 |
11 |
10 |
9 |
8 |
7 |
6 |
5 |
4 |
3 |
2 |
1 |
0 |
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
|
Manuf. specific |
Operation mode specific |
Internal limit active |
Target reached |
Remote |
Manuf. specific |
Warning |
Switch on disabled |
Quick stop |
Voltage enabled |
Fault |
Operation enabled |
Switched on |
Ready to switch on |
||
|
O |
O |
M |
M |
M |
O |
O |
M |
M |
M |
M |
M |
M |
M |
||
|
X |
X |
Max slippage error |
Speed |
X |
Target reached |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
|
Bit |
Name |
Value |
Description |
|---|---|---|---|
|
10 |
Target reached |
0 |
Halt = 0: Target Velocity not (yet) reached Halt = 1: Axle decelerates |
|
1 |
Halt = 0: Target Velocity reached Halt = 1: Velocity of axle is 0 |
||
|
12 |
Speed |
0 |
Not supported |
|
1 |
|||
|
13 |
Max slippage error |
0 |
Not supported |
|
1 |
Statusword for Cyclic Synchronous Position Mode (csp)
|
15 |
14 |
13 |
12 |
11 |
10 |
9 |
8 |
7 |
6 |
5 |
4 |
3 |
2 |
1 |
0 |
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
|
Manuf. specific |
Operation mode specific |
Internal limit active |
Target reached |
Remote |
Manuf. specific |
Warning |
Switch on disabled |
Quick stop |
Voltage enabled |
Fault |
Operation enabled |
Switched on |
Ready to switch on |
||
|
O |
O |
M |
M |
M |
O |
O |
M |
M |
M |
M |
M |
M |
M |
||
|
X |
X |
Following Error |
Target Position Ignored |
X |
Reserv. |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
|
Bit |
Name |
Value |
Description |
|---|---|---|---|
|
10 |
Reserved |
0 |
Reserved |
|
1 |
Reserved |
||
|
12 |
Target Position Ignored |
0 |
Target position ignored |
|
1 |
Target position shall be used as input to position control loop |
||
|
13 |
Following Error |
0 |
No following error |
|
1 |
Following error |
Statusword for Cyclic Synchronous Velocity Mode (csv)
|
15 |
14 |
13 |
12 |
11 |
10 |
9 |
8 |
7 |
6 |
5 |
4 |
3 |
2 |
1 |
0 |
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
|
Manuf. specific |
Operation mode specific |
Internal limit active |
Target reached |
Remote |
Manuf. specific |
Warning |
Switch on disabled |
Quick stop |
Voltage enabled |
Fault |
Operation enabled |
Switched on |
Ready to switch on |
||
|
O |
O |
M |
M |
M |
O |
O |
M |
M |
M |
M |
M |
M |
M |
||
|
X |
X |
Reserv. |
Target Velocity Ignored |
X |
Reserv. |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
|
Bit |
Name |
Value |
Description |
|---|---|---|---|
|
10 |
Reserved |
0 |
Reserved |
|
1 |
Reserved |
||
|
12 |
Target Velocity Ignored |
0 |
Target velocity ignored |
|
1 |
Target velocity shall be used as input to velocity control loop |
||
|
13 |
Reserved |
0 |
Reserved |
|
1 |
Reserved |
Statusword for Velocity Mode (vl)
|
15 |
14 |
13 |
12 |
11 |
10 |
9 |
8 |
7 |
6 |
5 |
4 |
3 |
2 |
1 |
0 |
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
|
Manuf. specific |
Operation mode specific |
Internal limit active |
Target reached |
Remote |
Manuf. specific |
Warning |
Switch on disabled |
Quickstop |
Voltageenabled |
Fault |
Operationenabled |
Switchedon |
Ready to switch on |
||
|
O |
O |
M |
M |
M |
O |
O |
M |
M |
M |
M |
M |
M |
M |
||
|
X |
X |
reserved |
reserved |
X |
reserved |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
Statusword for Profile Torque Mode (tq)
|
15 |
14 |
13 |
12 |
11 |
10 |
9 |
8 |
7 |
6 |
5 |
4 |
3 |
2 |
1 |
0 |
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
|
Manuf. specific |
Operation mode specific |
Internal limit active |
Target reached |
Remote |
Manuf. specific |
Warning |
Switch on disabled |
Quick stop |
Voltage enabled |
Fault |
Operationenabled |
Switched on |
Ready to switch on |
||
|
O |
O |
M |
M |
M |
O |
O |
M |
M |
M |
M |
M |
M |
M |
||
|
X |
X |
reserved |
reserved |
X |
Target reached |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
|
Bit |
Name |
Value |
Description |
|---|---|---|---|
|
10 |
Target reached |
0 |
Halt (bit8 Controlword) = 0; Target torque not reached Halt (bit8 Controlword) = 1; Axis decelerates |
|
1 |
Halt (bit8 Controlword) = 0; Target torque reached Halt (bit8 Controlword) = 1; Velocity of axis is 0 |
Statusword for Cyclic Synchronous Torque Mode (cst)
|
15 |
14 |
13 |
12 |
11 |
10 |
9 |
8 |
7 |
6 |
5 |
4 |
3 |
2 |
1 |
0 |
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
|
Manuf. specific |
Operation mode specific |
Internal limit active |
Target reached |
Remote |
Manuf. specific |
Warning |
Switch on disabled |
Quick stop |
Voltage enabled |
Fault |
Operation enabled |
Switched on |
Ready to switch on |
||
|
O |
O |
M |
M |
M |
O |
O |
M |
M |
M |
M |
M |
M |
M |
||
|
X |
X |
reserved |
Drive follows the command value |
X |
reserved |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
|
Bit |
Name |
Value |
Description |
|---|---|---|---|
|
12 |
Drive follows the command value |
0 |
Drive does not follow the command value – Target torque ignored |
|
1 |
Drive follows the command value – Target torque used as input to control loop |
Statusword for Feedback Sensor Calibration Mode (fsc)
|
15 |
14 |
13 |
12 |
11 |
10 |
9 |
8 |
7 |
6 |
5 |
4 |
3 |
2 |
1 |
0 |
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
|
Manuf. specific |
Operation mode specific |
Internal limit active |
Target reached |
Remote |
Manuf. specific |
Warning |
Switch on disabled |
Quick stop |
Voltage enabled |
Fault |
Operation enabled |
Switched on |
Ready to switch on |
||
|
O |
O |
M |
M |
M |
O |
O |
M |
M |
M |
M |
M |
M |
M |
||
|
X |
Calibration Error |
Calibration attained |
Calibration in progress |
X |
reserved |
X |
X |
X |
X |
X |
X |
X |
X |
X |
X |
|
Bit |
Name |
Value |
Description |
|---|---|---|---|
|
12 |
Calibration in progress |
0 |
Feedback Sensor Calibration procedure not active |
|
1 |
Feedback Sensor Calibration procedure is in progress |
||
|
13 |
Calibration attained |
0 |
Feedback Sensor Calibration procedure not attained |
|
1 |
Feedback Sensor Calibration attained |
||
|
14 |
Calibration error |
0 |
Feedback Sensor Calibration procedure not active or in progress or not yet attained |
|
1 |
Feedback Sensor Calibration Error |